Controlling the Write Address When Writing Image to External Memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Controlling the Write Address When Writing Image to External Memory

1,466件の閲覧回数
samxiao
Contributor I

I have questions about controlling the address of i.MX6 dual lite (the one with EPDC controller in it) when writing an image of 1600x2400 to external memory. Which module is in charge of generating the write image address? SDMA or MMDC? Can either of this module generate 2D address which line offset exists between image lines?

ラベル(1)
0 件の賞賛
返信
1 返信

1,402件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sam

PXP module has own dma engine and it provides data processing

for EPDC.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信