Controlling i.MX8M Nano Cortex-M7 from linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Controlling i.MX8M Nano Cortex-M7 from linux

2,017 Views
andreas2
Contributor I

Hi,

Are there any software similar to m4ctrl/m4fwload available for the imx8m Nano which uses a Cortex-M7 instead of a Cortex M4 ? I have been looking all over, but I am unable to see much information about this. In my current design I would need to be able to start/stop and reprogram the M7 from linux without rebooting to u-boot. It would be nice if someone has looked into this, or if there is some software I have missed.

0 Kudos
Reply
1 Reply

1,968 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Andreas,

I think is better to use the MX8Mmini for this task. The m4ctrl is not available on nano.

Regards

0 Kudos
Reply