Controlling GPIO in Android for i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Controlling GPIO in Android for i.MX6

跳至解决方案
12,210 次查看
krzysztofsza_ac
Contributor III

Hello!

Now we're trying to controll GPIO ports from Android.

Let's say we have connected LED to GPIO1[7].

What we've done till now:

1. Added MX6Q_PAD_GPIO7__GPIO_1_7 to mx6q_var_som_pads array in /kernel_imx/arch/arm/mach-mx6/board-mx6q_var_som.h

2. Builded kernel (step 6.7 from http://variwiki.com/index.php?title=VAR-SOM-MX6_Android_GS_R21)

3. Builded boot.img (step 6.4 from VAR-SOM-MX6 Android GS R21 - Variscite Wiki)

(nexts steps were made on android root console)

4. Checked if GPIO are available in FS (we have gpiochipxx available in /sys/class/gpio) and exported GPIO7 (echo 7 > /sys/class/gpio/export)

5. Changed direction to out for GPIO7 (echo out > /sys/class/gpio7/direction)

6. Tried to drive the LED connected to this GPIO, but with no luck (echo 1 > /sys/class/gpio7/value or echo 0 > /sys/class/gpio7/value)

Have we missed some steps?

标签 (2)
1 解答
10,297 次查看
krzysztofsza_ac
Contributor III

Hi Igor! Just want to let you know that I'va managed to control GPIO, for now output only, but it's going right direction.

Main problem was with IOMUX in board-mx6q_var_som.h. I've muxed some of them to be GPIO but didn't check that below they were used as other lines :smileyhappy: No I'm testing GPIO3[22] and exporting this as a GPIO86 works fine. Thanks! Now I'm also trying to access UART3, but this is other story...

在原帖中查看解决方案

0 项奖励
回复
16 回复数
10,297 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Krzysztof

I think it should be like (/gpio/gpio7) :

echo out > /sys/class/gpio/gpio7/direction

as described in

Re: GPIO access

Working with GPIO on the Wandboard and Writing an Android Driver for GPIO Interrupts | Using Android...

Best regards

igor

0 项奖励
回复
10,297 次查看
krzysztofsza_ac
Contributor III

You're right, but it was mistake only in creating post on forum :smileyhappy: Thanks for pointing this out.

Of course we use /sys/class/gpio/gpio7/ not /sys/class/gpio7/ - so this wasn't couse of the problem.

0 项奖励
回复
10,297 次查看
igorpadykov
NXP Employee
NXP Employee

One can try other pins to check if this works on this board or check GPIO/IOMUX registers with

memtool

Re: How to confirm a Register value on AndroidKK4.4.2 for MX6-SABRE-SD

~igor

10,297 次查看
krzysztofsza_ac
Contributor III

Will this patch also work for Android 4.2.2?

0 项奖励
回复
10,297 次查看
igorpadykov
NXP Employee
NXP Employee

I think yes.

0 项奖励
回复
10,297 次查看
krzysztofsza_ac
Contributor III

Well, maybe I've made some mistake but:

- I've copied this patch file to jb_422_110_build/external/linux-test/

- git apply this path (success)

- checked, that Android.mk was added to test/memtool

- rebuild all sources (make from jb_422_110_build directory)

- reflashed SOM

But memtool wasn't found as android command?

root@android:/ # memtool

/system/bin/sh: memtool: not found

0 项奖励
回复
10,297 次查看
igorpadykov
NXP Employee
NXP Employee

what is about test/memtool folder ?

0 项奖励
回复
10,297 次查看
krzysztofsza_ac
Contributor III

Are you asking what's inside jb_422_110_build/external/linux-test/test/memtool folder?

If so:

- Android.mk

- Makefile

- memtool.c

- memtools_register_info.h

- mx6dl_modules.c

- mx6q_modules.c

- mx6sl_modules.c

0 项奖励
回复
10,297 次查看
igorpadykov
NXP Employee
NXP Employee

after compilation there should be executable

0 项奖励
回复
10,297 次查看
krzysztofsza_ac
Contributor III

Hello igorpadykov

I've finally added memtool to my android compilation.

Let's say I want to test switch connected to GPIO3[23]/UART3_CTS - how can I do it?

First I check address of GPIO3.PSR2 (memtool GPIO3.PSR23):

     GPIO3     Addr:0x20a4000

Then I call memtool -32 0x20a4000 1

     Reading 0x1 count starting at address 0x20a4000

     0x20a4000:     4C1F2080

I push switch, call once again the same and... result is the same.

0 项奖励
回复
10,297 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Krzysztof

one can set GPIO direction register (GPIOx_GDIR)

as input, for PSR check below

Is gpio_get_value() working correctly?

~igor

10,297 次查看
krzysztofsza_ac
Contributor III

Hi Igor, thanks for suggestion.

First I've checked base addr of GPIO3 direction register:

    root@android:/ # memtool GPIO3.GDIR

     SOC is mx6q

     GPIO3    Addr:0x20a4000

       GPIO3.GDIR Addr:0x020A4004 Value:0x10002000 - GPIO_GDIR functions as direction control when the IOMUXC is in GPIO mode.

          GPIO3.GDIR.GDIR(0..31)     :0x10002000

                  GPIO direction bits.

I've changed GPIO3.23 direction to input:

     root@android:/ # memtool -32 0x020A4004=0x189E50

     Writing 32-bit value 0x189E50 to address 0x020A4004

Then I've checked if it has written:

     root@android:/ # memtool GPIO3.GDIR

     SOC is mx6q

     GPIO3    Addr:0x20a4000

       GPIO3.GDIR Addr:0x020A4004 Value:0x00189E50 - GPIO_GDIR functions as direction control when the IOMUXC is in GPIO mode.

          GPIO3.GDIR.GDIR(0..31)     :0x189e50

                  GPIO direction bits.

Get value from GPIO3:

     root@android:/ # memtool GPIO3.DR

     SOC is mx6q

     GPIO3    Addr:0x20a4000

       GPIO3.DR Addr:0x020A4000 Value:0x4C1F0080 - The 32-bit GPIO_DR register stores data that is ready to be driven to the output lines.

          GPIO3.DR.DR(0..31)         :0x4c1f0080

                  Data bits.

Push button, check the same - still the same value (0x4c1f0080).

Maybe I'm refereing to wrong IO port? I've connected button to GPIO3[23]/UART3_CTS. Button is shorting IO line to GND. Should I setup a pullup somehow?

0 项奖励
回复
10,297 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Krzysztof

I would suggest to attach jtag debugger and

try to check this GPIO. Also one can check all register settings.

~igor

0 项奖励
回复
10,297 次查看
krzysztofsza_ac
Contributor III

Oh, this is something new for me as I'm rather software developer :smileyhappy: Can you suggest some software? And we have JTAG J-Link Ultra+ - will it be sufficient?

0 项奖励
回复
10,297 次查看
igorpadykov
NXP Employee
NXP Employee

Yes, J-Link jtag will support i.MX6.

Also IAR Embedded Workbench 7.0 has i.MX6 examples (led blink)

and you can easily simulate your settings. Then

you can printf Android settings and compare them.

~igor

0 项奖励
回复
10,298 次查看
krzysztofsza_ac
Contributor III

Hi Igor! Just want to let you know that I'va managed to control GPIO, for now output only, but it's going right direction.

Main problem was with IOMUX in board-mx6q_var_som.h. I've muxed some of them to be GPIO but didn't check that below they were used as other lines :smileyhappy: No I'm testing GPIO3[22] and exporting this as a GPIO86 works fine. Thanks! Now I'm also trying to access UART3, but this is other story...

0 项奖励
回复