Control Register configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Control Register configuration

1,568件の閲覧回数
dhanushvenugopa
Contributor I

Hi,

I am using the imx6ul evk board with yocto 4.9.x version ,since i need more number of gpio's I'm tring to mux the ethernet pins ,what value need to be set in the control register, so that the pin gets toggled with the voltage 0 and 3.3v when the  pin is made low and high respectively

ラベル(1)
0 件の賞賛
返信
1 返信

1,485件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Dhanush

for i.MX6UL gpio control one can look at

Simple GPIO Example - quandry 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信