Connect iMX8M Mini with WinSCP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connect iMX8M Mini with WinSCP

1,781 Views
inigovicentewal
Contributor III

Hi,

How can I connect my imx8m Mini board with winscp if I don't have the server's ip?

Labels (1)
0 Kudos
Reply
2 Replies

1,694 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can boot up your board first, and then see your board IP address. Then you can try the following thread https://community.nxp.com/message/1126058 check to make the winscp work.

0 Kudos
Reply

1,694 Views
inigovicentewal
Contributor III

I have the image obtained from here: L4.14.98_2.0.0_ga_images_MX8MMEVK
It has dropbear ssh, but it is enabled, how do I know that ssh is running? The IP is in the same subnet.

0 Kudos
Reply