imx6ull is not reachable via TCP/IP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull is not reachable via TCP/IP

3,015 Views
sneha_raghunand
Contributor II

The command ifconfig yields a valid ip address, but scp using the same ip address, results in time out. See attached image

scp does not work via linux terminal in Ubuntu and also with winSCP

Labels (1)
0 Kudos
Reply
2 Replies

2,902 Views
b36401
NXP Employee
NXP Employee

First please make sure that routing is OK between PC and i.MX.
If they are in the same segment of LAN (usual case) you need to make sure that IP addresses are in the same subnet (for example 192.168.0.2 and 192.168.0.3) and this subnet is added to routing table.

Then please make sure that you can ping one host from another.

If all above is OK you need to make sure that ssh server is running on i.MX.
You can check if some server listens to post 22 this way:
# netstat -na|grep LISTEN
And then you can try to connect ssh from the board itself:
# ssh localhost

0 Kudos
Reply

2,902 Views
inigovicentewal
Contributor III

Hi @VictorLinnik,

What settings must be done in yocto to enable ssh? How do I know what is enabled?

I compiled the image whith IMAGE_INSTALL_append+= " openssh" but I can't connect with winscp.

Any idea?

Thanks.

0 Kudos
Reply