Connect iMX8M Mini with WinSCP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connect iMX8M Mini with WinSCP

1,779件の閲覧回数
inigovicentewal
Contributor III

Hi,

How can I connect my imx8m Mini board with winscp if I don't have the server's ip?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,692件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

You can boot up your board first, and then see your board IP address. Then you can try the following thread https://community.nxp.com/message/1126058 check to make the winscp work.

0 件の賞賛
返信

1,692件の閲覧回数
inigovicentewal
Contributor III

I have the image obtained from here: L4.14.98_2.0.0_ga_images_MX8MMEVK
It has dropbear ssh, but it is enabled, how do I know that ssh is running? The IP is in the same subnet.

0 件の賞賛
返信