Connect USB 3.0 camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connect USB 3.0 camera

1,995 Views
hmartinez
Contributor I

Hello,

I am trying to connect a USB camera to the MCIMX8M-EVK, but it does not recognise it. The only thing that appears is:

usb 2-1: new SuperSpeed USB device number 2 using xhci-hcd

But no further messages of detection are shown. Is there any specific Linux image I can use to make it work? I have tried with L4.9.88_2.0.0_images_MX8MQ.


Thank you in advance!

Labels (1)
0 Kudos
Reply
1 Reply

1,938 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Hector,

The message

usb 2-1: new SuperSpeed USB device number 2 using xhci-hcd


Means that is recognized, just mount the USB.

Regards

0 Kudos
Reply