Configuringb IP data NET Stack

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuringb IP data NET Stack

Jump to solution
8,849 Views
lyfsci
Contributor III

Hi Experts,

Consider I am configuring the Ethernet connectivity manually to connect with the static connection.


"I am not using the dhcp connection".

How to configure the NET stack ?

I am using the following steps.


1. ifconfig eth0 inet <ip_addr> netmask <broadcast>

2. route add default gw

My expectation is if I configure the above things then the IP data started flowing.

Labels (1)
0 Kudos
Reply
1 Solution
8,656 Views
igorpadykov
NXP Employee
NXP Employee

Hi lyf

suggest to look at attached Release Notes Table 5-1. Kernel Boot Parameters,

Linux BSP UserGuide sect.8.1 Run the image from NFS and use

L2.6.35_11_09_ER_SOURCE : Linux 2.6.35 Source Code Files

Best regards

igor

View solution in original post

0 Kudos
Reply
5 Replies
8,656 Views
igorpadykov
NXP Employee
NXP Employee

Hi lyf

suggest to look at attached Release Notes Table 5-1. Kernel Boot Parameters,

Linux BSP UserGuide sect.8.1 Run the image from NFS and use

L2.6.35_11_09_ER_SOURCE : Linux 2.6.35 Source Code Files

Best regards

igor

0 Kudos
Reply
8,656 Views
lyfsci
Contributor III

Hi Igor,

Thanks for the reply.

I am not looking for the NFS or boot configurations rather than that I am

looking for static configuration to open the IP data exchange when it is

connected with the Server or PC which doesn't supports ARP/DHCP.

Regards,

Lyf

On Tue, Mar 3, 2015 at 10:31 AM, igorpadykov <[email protected]>

0 Kudos
Reply
8,656 Views
mbp
Contributor V

Lyf,

Were you ever able to get this going?   

What did you learn?

I'm trying to update our Mx51 BBG Android 2.3 to support static IP instead of just DHCP!

Any insight, pointers, links, etc. would be most welcome!    

thanks,

Mike

0 Kudos
Reply
8,656 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi lyd sci,

Which processor are you using and on which platform?
Have a great day
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
8,656 Views
lyfsci
Contributor III

Hi Dan,

I am using i.MX53 Quick Start Board.

Regards,

Lyf

0 Kudos
Reply