Configuringb IP data NET Stack

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuringb IP data NET Stack

ソリューションへジャンプ
8,840件の閲覧回数
lyfsci
Contributor III

Hi Experts,

Consider I am configuring the Ethernet connectivity manually to connect with the static connection.


"I am not using the dhcp connection".

How to configure the NET stack ?

I am using the following steps.


1. ifconfig eth0 inet <ip_addr> netmask <broadcast>

2. route add default gw

My expectation is if I configure the above things then the IP data started flowing.

ラベル(1)
0 件の賞賛
返信
1 解決策
8,647件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi lyf

suggest to look at attached Release Notes Table 5-1. Kernel Boot Parameters,

Linux BSP UserGuide sect.8.1 Run the image from NFS and use

L2.6.35_11_09_ER_SOURCE : Linux 2.6.35 Source Code Files

Best regards

igor

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
8,647件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi lyf

suggest to look at attached Release Notes Table 5-1. Kernel Boot Parameters,

Linux BSP UserGuide sect.8.1 Run the image from NFS and use

L2.6.35_11_09_ER_SOURCE : Linux 2.6.35 Source Code Files

Best regards

igor

0 件の賞賛
返信
8,647件の閲覧回数
lyfsci
Contributor III

Hi Igor,

Thanks for the reply.

I am not looking for the NFS or boot configurations rather than that I am

looking for static configuration to open the IP data exchange when it is

connected with the Server or PC which doesn't supports ARP/DHCP.

Regards,

Lyf

On Tue, Mar 3, 2015 at 10:31 AM, igorpadykov <[email protected]>

0 件の賞賛
返信
8,647件の閲覧回数
mbp
Contributor V

Lyf,

Were you ever able to get this going?   

What did you learn?

I'm trying to update our Mx51 BBG Android 2.3 to support static IP instead of just DHCP!

Any insight, pointers, links, etc. would be most welcome!    

thanks,

Mike

0 件の賞賛
返信
8,647件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi lyd sci,

Which processor are you using and on which platform?
Have a great day
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
8,647件の閲覧回数
lyfsci
Contributor III

Hi Dan,

I am using i.MX53 Quick Start Board.

Regards,

Lyf

0 件の賞賛
返信