Configuring the parallel camera IO pins.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuring the parallel camera IO pins.

ソリューションへジャンプ
3,829件の閲覧回数
camz
Contributor I

I'm helping design a board based on the i.MX6Q processor.

The design has a parallel camera that will use the Bayer/Raw data mode to receive 16-bits of camera data.

I have planned to use the CSI0_DAT0 thru CSI0_DAT15 inputs, but in looking at the Sabre for Smart Devices reference schematic, the connection of the OV5642 parallel camera uses CSI0_DAT12 thru CSI0_DAT19 for an 8-bit input stream.  When not using all 20-bits for input, should I be using the high bits, or the low bits?

The i.MX6Q reference manual skims over the various modes and leaves out a lot of details on how to configure and hook up camera inputs, if there is a document that describes this, I'd appreciate being pointed in the right direction.

Cheers,

Camz.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
3,605件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Martin

When not using all 20-bits for input, one should use the high bits.

Regarding docs please check i.MX_6Dual6Quad_BSP_Porting_Guide.pdf,

i.MX_6Dual6Quad_Linux_Reference_Manual.pdf

L3.0.35_4.1.0_LINUX_DOCS

For software examples it is better to look for Community.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,606件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Martin

When not using all 20-bits for input, one should use the high bits.

Regarding docs please check i.MX_6Dual6Quad_BSP_Porting_Guide.pdf,

i.MX_6Dual6Quad_Linux_Reference_Manual.pdf

L3.0.35_4.1.0_LINUX_DOCS

For software examples it is better to look for Community.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,605件の閲覧回数
camz
Contributor I

Awesome, thank you!

One other related question.

Although the camera interface will be operated in 16-bit mode, we only have 14 bits of data from the camera, so will be setting the two most-significant bits to 0.

If we instead just configure those pins for alternate functions, instead of connecting them to ground, what values would the camera interface read for those bits when they aren't physically connected to the pads via the IOmux?  We've almost run out of spare pins, so getting two more pins back for use as GPIOs would be fantastic.

Camz.

0 件の賞賛
返信
3,605件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Martin

I am afraid that internally they will be floating,

so camera interface will read random data for those bits.

Best regards

igor

3,605件の閲覧回数
camz
Contributor I

Thanks.

0 件の賞賛
返信