Configuring mma8653fc for freefall detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring mma8653fc for freefall detection

Jump to solution
1,774 Views
sandeepmantrala
Contributor I

Motion Detection - OK, Np

I am successfully able to configure MMA8653FC for motion detection using the data sheet.

Parameters are as follows :

FF_MT_THS  = 0x3F

ELE = 1 and OAE = 1

ZEFE = YEFE = XEFE = 1

Now I am trying to configure the sensor to detect freefalls and not motion

Works OK, without any issue

------------------------------------------------------------------------------------------------------------------

Freefall - Not ok :smileysad:

From data sheet, we need to configure the following values for freefall

ELE = 0 or 1 and OAE = 0

FF_MT_THS -> Contains a threshold value

From its description I see that

The unsigned 7-bit FF_MT_THS threshold register holds the threshold for the freefall detection where the magnitude of the X and Y and Z acceleration values is lower or equal than the threshold value.

From my understanding this means that if we have configured the threshold to +-4g, then whenever there is a acceleration lower than this threshold we will have an EA available in F_MT_SRC

So, even when the device is still, since 0 < 4g I always receive a freefall event. Which is obviously not right.

Q1 : So, I am not understanding how can I actually configure the parameters to correctly find a freefall event.

Q2: What is the difference between mode 1 and mode 2 as stated below

We have two modes to use for freefall. They say as follows :

Mode 1: Freefall detection with ELE = 0, OAE = 0

In this mode, the EA bit (0x16: FF_MTG_CFG, bit 7) indicates a freefall event after the debounce counter is complete.

Mode 2: Freefall detection with ELE = 1, OAE = 0

In this mode, the EA event bit indicates a freefall event after the debounce counter.

I don't understand what is the difference in both these statements..

0 Kudos
Reply
1 Solution
1,643 Views
sandeepmantrala
Contributor I

Hi David,

Thank you for the reply.

I read that part. What was confusing to me is that I initially thought when the device is falling, the acceleration is going to increase. Hence i configured my threshold that ways. But upon printing the raw values i noticed that the acceleration is decreasing and nearing to 0 when the device is falling.

I decreased the threshold and fixed the logic. Thank you

But when i printed the raw values, when the device is still, x y are 0 but z is about 1g and when its faling it is reducing and coming towards  0. So, I fixed the logic that ways.

Thank you.

View solution in original post

0 Kudos
Reply
2 Replies
1,643 Views
david_diaz
NXP Employee
NXP Employee

Hello Sandeep,

In order to get a better understanding of the Freefall detection, please review the application note below. At chapter 6.2, you may find a Example Steps for Configuring Linear Freefall Detection.

Motion and Freefall Detection Using the MMA8451, 2, 3Q

The ELE bit denotes whether the enabled event flag will to be latched in the FF_MT_SRC register or the event flag status in the FF_MT_SRC will indicate the real-time status of the event. If ELE bit is set to a logic ‘1’, then the event flags are frozen when the EA bit gets set, and are cleared by reading the FF_MT_SRC source register.

I hope this information helps.

Regards,

David

0 Kudos
Reply
1,644 Views
sandeepmantrala
Contributor I

Hi David,

Thank you for the reply.

I read that part. What was confusing to me is that I initially thought when the device is falling, the acceleration is going to increase. Hence i configured my threshold that ways. But upon printing the raw values i noticed that the acceleration is decreasing and nearing to 0 when the device is falling.

I decreased the threshold and fixed the logic. Thank you

But when i printed the raw values, when the device is still, x y are 0 but z is about 1g and when its faling it is reducing and coming towards  0. So, I fixed the logic that ways.

Thank you.

0 Kudos
Reply