Configuring SPI as Slave on IMX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Configuring SPI as Slave on IMX6

2,048 次查看
mahmood_md
Contributor I

Dear Members,

We are configuring SPI as slave mode on IMX6.

We have applied below patch to support SPI as slave mode How to support spi slave in kernel4.1.15 & imx6? 

patch file name imx_add_spi_slave_mode.path.zip

SPI master is a controller board, whenever the master sends data to the SPI slave, we do not see any event/data at slave side.

Can you please help us to tell how to proceed at the SPI slave side, that we can come to know data has arrived. 

Thanks,

Mahmood

标签 (3)
0 项奖励
回复
1 回复

1,911 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mahmood

one can try with baremetal ecspi test, and then compare settings with linux

rt-thread/bsp/imx6sx/iMX6_Platform_SDK/sdk/drivers/spi at master · RT-Thread/rt-thread · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复