Configuring Qt5.3.2 with X11

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuring Qt5.3.2 with X11

2,555件の閲覧回数
chaitanyad
Contributor I

Hello,

          I wish to configure QT5.3.2 with X11 on imx6 solo based custom platform. I followed the steps on

http://wiki.wandboard.org/Integrate_Qt5_into_yocto_sato_image_on_Wandboard  .

The build goes through but qt applications with qml give errors like : Unable to find an X11 visual which matches EGL config 28

I have also confirmed that Force egl visual ID 33.patch is also getting applied.

Any suggestions would be of help.

Thanks,

Chaitanya D

ラベル(5)
0 件の賞賛
返信
3 返答(返信)

2,134件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

2,133件の閲覧回数
chaitanyad
Contributor I

Hello,

            I tried this patch. Its not getting applied. Its failing in do_patch(). In qt 5.3.2, we do not have a "egl" folder under "src/gui/". Sine the patch tries to make changes in the path /src/giu/egl/qegl_x11.cpp which is not existant, it is failing.

Any more help will be appreciated.

Thanks,

Chaitanya Dhere

0 件の賞賛
返信

2,133件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I think if the error still exist, you may try to find the string "Unable to find an X11 visual which matches EGL" in the source code. Then modify the return ID to 33.

0 件の賞賛
返信