Configuring KSZ8795

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
7,461件の閲覧回数
aliismail
Contributor IV

Working on a custom board that uses imx6dqscm. We are using the KS8795 switch and having issues with configuring the ethernet. First, we are using the micrel driver, however, it does not seem to support the KS8795 switch. Does anyone know where we can find this driver or a patch? Also, if anyone knows of documentation that can give general guidance to setting up the ethernet?

Thanks!

ラベル(3)
0 件の賞賛
返信
1 解決策
5,093件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ali

one can look at driver at

http://lxr.free-electrons.com/source/drivers/net/phy/spi_ks8995.c
https://kernel.googlesource.com/pub/scm/linux/kernel/git/next/linux-next/+/refs/heads/akpm-base/Docu...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
5,094件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ali

one can look at driver at

http://lxr.free-electrons.com/source/drivers/net/phy/spi_ks8995.c
https://kernel.googlesource.com/pub/scm/linux/kernel/git/next/linux-next/+/refs/heads/akpm-base/Docu...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
5,094件の閲覧回数
eric_kang1
Contributor I

Hi Igor,

Long time no see.

I have a question for the RGMII connection between i.MX6Q and KSZ8795 Ethernet Switch.

I have to connect the both via RGMII Interface.

But I couldn't find how to connect the both.

Could you give me any reference schematic for that?

It's very helpful to me if i have that.

Best Regards,

Eric.

0 件の賞賛
返信
5,094件の閲覧回数
stevenguzior
Contributor I

It looks like this driver configures the PHY over SPI.  Is it possible to configure the PHY over MDIO using this driver and binding?

0 件の賞賛
返信