Configuring Display Interface For a new LCD(i.MX53).

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuring Display Interface For a new LCD(i.MX53).

ソリューションへジャンプ
2,887件の閲覧回数
ricardo_ioct
Contributor III

Hello, Community.

Recently, I'm trying to interface a Trully LCD. It's a 240x320(portrait) display, with RGB666 interface, VSYNC, HSYNC, PIXCLK and DE signals. Looking for references on Linux kernel(on arch files of the QSB board and SABRE), and reading IMX53 User Manual, I figured out that some pins of the DI module(DI0_PINxx) can act as VSYNC, HSYNC and DE, but I don't realize where in the BSP each generic pin is assigned with a specific function. Can someone help me?

For the record: on mx53_loco.c file, those pads are configured as sync pins:

MX53_PAD_DI0_PIN15__IPU_DI0_PIN15,
MX53_PAD_DI0_PIN2__IPU_DI0_PIN2,
MX53_PAD_DI0_PIN3__IPU_DI0_PIN3,

On QSB schematic, they are, respectively, DE, HSYNC and VSYNC. As these IPU pins are generics, I want to know where they are specifically configured.

Regards,

Ricardo Gurgel.

ラベル(2)
0 件の賞賛
返信
1 解決策
2,090件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

1. http://cache.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Please read the Chapter 18 for LCD porting details.

2.  Different Display Configurations on i.MX35 Linux PDK

http://cache.freescale.com/files/dsp/doc/app_note/AN3974.pdf

Although this is for i.MX35, the driving porting in Linux for i.MX53 is the same.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,091件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

1. http://cache.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Please read the Chapter 18 for LCD porting details.

2.  Different Display Configurations on i.MX35 Linux PDK

http://cache.freescale.com/files/dsp/doc/app_note/AN3974.pdf

Although this is for i.MX35, the driving porting in Linux for i.MX53 is the same.

0 件の賞賛
返信