Configure SNVS Power Key

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configure SNVS Power Key

3,052 Views
sandheepkumar
Contributor I


Hi All,

We would like to configure the button press time of SNVS Power Key in our custom iMX6 board. For this, we tried to access the 'BTN_PRESS_TIME' bits available in SNVS_LPCR Register but we are not able to update the register. Reference Manual states that these bits are read/write accessible but the Security Reference Manual states these bits are reserved.

Are those bits in SNVS_LPCR are read/write accessible ? Is there anyother way to disable the SNVS Power Key?

Thanks,

Sandheep

Labels (3)
Tags (2)
0 Kudos
Reply
1 Reply

2,531 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sandheep

PRESS_TIME field is not writeable and

I am afraid there is no way to disable SNVS Power Key

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply