Configure NXP i.MX8M Mini as PCIe Endpoint

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configure NXP i.MX8M Mini as PCIe Endpoint

2,682 Views
knoelker
Contributor I

Hi,

we have a Variscite evaluation board which includes an i.MX8M Mini. We want to use this as PCIe endpoint, so we have connected it to our host PC using a crossover cable. But in the host PC the i.MX8M Mini is not detected as PCIe device.

How can we configure the i.MX8M Mini as PCIe endpoint?

In the reference manual I only found that the bits 15-12 of "General Purpose Register 12" should probably be set to zero. Is this the way to go?

Thanks for any advice!

Labels (1)
0 Kudos
Reply
3 Replies

2,604 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Thorsten,

You should try the error description and explanations are provided on

pcie failed with error -110 - Toradex Community 

Regards

0 Kudos
Reply

2,604 Views
knoelker
Contributor I

I don't see anything useful in the dmesg output, also imx-pcie does not appear.

How can I configure it as PCIe endpoint? Or should it be detected out of the box?

0 Kudos
Reply

2,604 Views
knoelker
Contributor I

Any further advice???

0 Kudos
Reply