Configuration ESAI for GPIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuration ESAI for GPIO

3,688 Views
luongnguyen
Contributor II

now i'm working with I.MX6, With Enhanced Serial Audio Interface (ESAI), could you help me configure ESAI for GPIO by terminal or code,

Thank you so much,

Labels (2)
5 Replies

3,388 Views
igorpadykov
NXP Employee
NXP Employee

Hi Luong

probably you can use memtool, for usage one can look at

p.39 http://www.freescale.com/files/32bit/doc/app_note/AN4576.pdf

and change IOMUX registers for ESAI pads, check:

Chapter 4 External Signals and Pin Multiplexing

Chapter 28 General Purpose Input/Output (GPIO)

Chapter 36 IOMUX Controller (IOMUXC)

IMX6DQRM i.MX 6Dual/6Quad Applications Processor Reference Manual

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

3,388 Views
luongnguyen
Contributor II

Hello Igorpadykov,

Thank you very much, your reply is really helpful for me,

i'm a new guide for ARM A9 and linux, last night, i spent more time to  read for understand the document of GPIO and IOMUX, but i don't know the Memtool, could you help a Memtool for I.MX6Q, and my OS is debian,


Thanks and regards,

Luong Nguyen,


P/s: Thank you again for the time, 

0 Kudos
Reply

3,388 Views
igorpadykov
NXP Employee
NXP Employee

Hi Luong

you can find it in Demo images or after building Linux sources

L3.0.35_4.1.0_DEMO_IMAGE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux Binary Demo Files.

L3.0.35_4.1.0_ER_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.

http://svn.slimdevices.com/repos/jive/7.8/trunk/squeezeos/src/jivetest/memtool.c

Best regards

igor

3,388 Views
luongnguyen
Contributor II

Dear Igorpadykov,

i use iomux_tool_v3.4.0.3 for creat library and code for change mode of GPIO1_IO2 and  GPIO1_IO09, i choose device is I.M6DQ,

the function gpio1_iomux_config():

HW_IOMUXC_SW_MUX_CTL_PAD_GPIO02_WR(

            BF_IOMUXC_SW_MUX_CTL_PAD_GPIO02_SION_V(DISABLED) |

            BF_IOMUXC_SW_MUX_CTL_PAD_GPIO02_MUX_MODE_V(ALT5));

HW_IOMUXC_SW_PAD_CTL_PAD_GPIO02_WR(

            BF_IOMUXC_SW_PAD_CTL_PAD_GPIO02_HYS_V(ENABLED) |

            BF_IOMUXC_SW_PAD_CTL_PAD_GPIO02_PUS_V(100K_OHM_PU) |

            BF_IOMUXC_SW_PAD_CTL_PAD_GPIO02_PUE_V(PULL) |

            BF_IOMUXC_SW_PAD_CTL_PAD_GPIO02_PKE_V(ENABLED) |

            BF_IOMUXC_SW_PAD_CTL_PAD_GPIO02_ODE_V(DISABLED) |

            BF_IOMUXC_SW_PAD_CTL_PAD_GPIO02_SPEED_V(100MHZ) |

            BF_IOMUXC_SW_PAD_CTL_PAD_GPIO02_DSE_V(40_OHM) |

            BF_IOMUXC_SW_PAD_CTL_PAD_GPIO02_SRE_V(SLOW));

all of my test project in a link http://www.mediafire.com/download/4912tz975u06s10/GPIO29.rar, i use eclipse,

but when i runt it, the notification is: Segmentation fault

could you help me?

Thanks and regard,

Luong Nguyen,

0 Kudos
Reply

3,388 Views
igorpadykov
NXP Employee
NXP Employee

Hi Luong

for bare metal tests please try SDK

i.MX 6Series Platform SDK : Bare-metal SDK for the i.MX 6 series

~igor

0 Kudos
Reply