ConfigTools for i.MX Version 9.0 Constraints

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ConfigTools for i.MX Version 9.0 Constraints

2,617 次查看
ban45
Contributor III

Hi

 

I was able to set the pin without displaying an error.
I would like to understand the mistakes when using ConfigTools.

I heard that switching only the CTS and RTS functions does not work.
I would like to know why the error did not occur even though I exchanged only the CTS function and RTS function of UART communication.

Can ConfigTools for i.MX version 9.0 reflect register settings?

Is there no register constraint and does error checking only check if a feature can be assigned?

I would appreciate it if you could tell me where you suspect a mistake in usage.

best regard.

0 项奖励
回复
3 回复数

2,580 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport
0 项奖励
回复

2,573 次查看
ban45
Contributor III

Hi b45499.

I.MX6 is not included in ConfigTools for i.MX Version 10.0.

What and how should I add it?

best regard.

0 项奖励
回复

2,563 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

You can using the Pins tool to generate it. Select to "Create a new configuration for a borad or porcessor", then select the what you need.

0 项奖励
回复