ConfigTools for i.MX Version 9.0 Constraints

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ConfigTools for i.MX Version 9.0 Constraints

2,592 Views
ban45
Contributor III

Hi

 

I was able to set the pin without displaying an error.
I would like to understand the mistakes when using ConfigTools.

I heard that switching only the CTS and RTS functions does not work.
I would like to know why the error did not occur even though I exchanged only the CTS function and RTS function of UART communication.

Can ConfigTools for i.MX version 9.0 reflect register settings?

Is there no register constraint and does error checking only check if a feature can be assigned?

I would appreciate it if you could tell me where you suspect a mistake in usage.

best regard.

0 Kudos
Reply
3 Replies

2,555 Views
Rita_Wang
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,548 Views
ban45
Contributor III

Hi b45499.

I.MX6 is not included in ConfigTools for i.MX Version 10.0.

What and how should I add it?

best regard.

0 Kudos
Reply

2,538 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can using the Pins tool to generate it. Select to "Create a new configuration for a borad or porcessor", then select the what you need.

0 Kudos
Reply