Compile u-boot_v2017 for use with MFG-Tool in standalone environment

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Compile u-boot_v2017 for use with MFG-Tool in standalone environment

1,467 次查看
oliverpenzler
Contributor I

I'm trying to compile u-boot from branch imx_v2017.03_4.9.51_imx8_beta2 for my custom i.MX 6 Dual target board.

So far I've found the attached document from the following link:

https://community.nxp.com/thread/323039

But the provided instructions seem to be outdated, as I get the following error from the MFG-Tool:

"Boot" body="BootStrap" error, file="D:\mfg\Profiles\REVB\OS Firmware\mfgimages\u-boot.bin"

I've also attached the error log from the MFG-Tool.

I'm not looking for instructions using the Yocto-Toolchain but using a standalone environment.

What are the necessary steps to compile imx u-boot v2017 for the MFG-Tool?

Thanks in advance.

标签 (1)
0 项奖励
回复
1 回复

1,325 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we do not have BSP support with the Linux version 4.9.51 for the i.MX6D. This BSP was released only for the i.MX8MQ, I apologize for the inconveniences.

Best Regards,

Diego.

0 项奖励
回复