Compile fail occur(bitbake fsl-image-mfgtool-initramfs)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compile fail occur(bitbake fsl-image-mfgtool-initramfs)

Jump to solution
2,414 Views
suehyun_lee
Contributor I

Hi , I am trying to flash image using the UUU tool.

When flashing an image using the UUU tool, can I use "fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot" in the sample. (I am using sample - L4.19.35_1.1.0_images_MX8MQEVK)

Or should I build "fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot"?

If I try to build with below command, some errors occur.

$bitbake fsl-image-mfgtool-initramfs

Errors are about imx-uuc and imx-kobs.

1 Solution
2,269 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot is for uuu, you can use the default one, no need to build for it again.

View solution in original post

3 Replies
2,270 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot is for uuu, you can use the default one, no need to build for it again.

2,269 Views
suehyun_lee
Contributor I

Thanks

Using default one, flash succeeded.

0 Kudos
Reply
2,269 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

OK

0 Kudos
Reply