Compile fail occur(bitbake fsl-image-mfgtool-initramfs)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Compile fail occur(bitbake fsl-image-mfgtool-initramfs)

跳至解决方案
2,437 次查看
suehyun_lee
Contributor I

Hi , I am trying to flash image using the UUU tool.

When flashing an image using the UUU tool, can I use "fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot" in the sample. (I am using sample - L4.19.35_1.1.0_images_MX8MQEVK)

Or should I build "fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot"?

If I try to build with below command, some errors occur.

$bitbake fsl-image-mfgtool-initramfs

Errors are about imx-uuc and imx-kobs.

1 解答
2,292 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot is for uuu, you can use the default one, no need to build for it again.

在原帖中查看解决方案

3 回复数
2,293 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

The fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot is for uuu, you can use the default one, no need to build for it again.

2,292 次查看
suehyun_lee
Contributor I

Thanks

Using default one, flash succeeded.

0 项奖励
回复
2,292 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

OK

0 项奖励
回复