Compilation of opencv with OpenGL on imx95 eval board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Compilation of opencv with OpenGL on imx95 eval board

492 次查看
Tuitor
Contributor II

Dear NXP community,

I'm trying to build a full image for imx95 eval board using

- manifest: imx-6.12.20-2.0.0.xml

- machine: imx95-19x19-verdin

- distro: fsl-imx-xwayland

Without any modification in the recipes, the build is successful, but then I need to compile opencv using openGL. So I added the WITH_OPENGL=ON flag to my opencv.bbappend recipe, but it seems there is no OpenGL ES user-space driver/headers for i.MX95 in the Yocto setup right now.

Can anybody confirm ? Is it planned to be added ?

thank you

标记 (3)
0 项奖励
回复
1 回复

475 次查看
Chavira
NXP TechSupport
NXP TechSupport

HI @Tuitor!


As the i.MX95 is currently in the pre-production stage, we are actively working to integrate all GPU features into the BSP.

Best regards,
Chavira