Compilation of opencv with OpenGL on imx95 eval board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compilation of opencv with OpenGL on imx95 eval board

493件の閲覧回数
Tuitor
Contributor II

Dear NXP community,

I'm trying to build a full image for imx95 eval board using

- manifest: imx-6.12.20-2.0.0.xml

- machine: imx95-19x19-verdin

- distro: fsl-imx-xwayland

Without any modification in the recipes, the build is successful, but then I need to compile opencv using openGL. So I added the WITH_OPENGL=ON flag to my opencv.bbappend recipe, but it seems there is no OpenGL ES user-space driver/headers for i.MX95 in the Yocto setup right now.

Can anybody confirm ? Is it planned to be added ?

thank you

タグ(3)
0 件の賞賛
返信
1 返信

476件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

HI @Tuitor!


As the i.MX95 is currently in the pre-production stage, we are actively working to integrate all GPU features into the BSP.

Best regards,
Chavira