Compilation error got on Sabre Platform (i.MX 6Quad)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compilation error got on Sabre Platform (i.MX 6Quad)

ソリューションへジャンプ
1,852件の閲覧回数
bipinkumar
Contributor I

I am trying to compile the Android source code (Android - 5.0.2). But i m getting the compilation error. Although i have added the patch file and followed the steps form the Android_User's_Guide PDF downloaded. So can anyone help regarding this so that i can proceed further. For reference i have attached the log file which i got during the compilation.

 

make[1]: Entering directory `/home/db810/sabre_platform/Android-5.0.2_r1/bootable/bootloader/uboot-imx'
rm: cannot remove ‘arch/arm/include/asm/arch’: Is a directory
rm: cannot remove ‘arch/arm/include/asm/proc’: Is a directory
make[1]: *** [mrproper] Error 1
make[1]: Leaving directory `/home/db810/sabre_platform/Android-5.0.2_r1/bootable/bootloader/uboot-imx'
make[1]: Entering directory `/home/db810/sabre_platform/Android-5.0.2_r1/bootable/bootloader/uboot-imx'
Configuring for mx6qsabresdandroid - Board: mx6sabresd, Options: IMX_CONFIG=board/freescale/imx/ddr/mx6q_4x_mt41j128.cfg,MX6Q,DEFAULT_FDT_FILE="imx6q-sabresd.dtb",DDR_MB=1024,SYS_USE_SPINOR,ANDROID_SUPPORT
rm: cannot remove ‘asm/arch’: Is a directory
make[1]: *** [mx6qsabresdandroid_config] Error 1

Original Attachment has been moved to: build-log.txt.zip

0 件の賞賛
返信
1 解決策
1,681件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please use NXP Android packages from the Web

i.MX 6 Series Software and Development Tool|NXP 

I do not see 5.0.2 release there.


android.jpg

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

元の投稿で解決策を見る

1 返信
1,682件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please use NXP Android packages from the Web

i.MX 6 Series Software and Development Tool|NXP 

I do not see 5.0.2 release there.


android.jpg

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!