Communicate with FLEXCAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Communicate with FLEXCAN

1,628件の閲覧回数
kishorekrish
Contributor I

Hi,

I have IMX6 sabrelite board and it has CAN controller and Transceiver as well, I am tested CAN interface between 2 IMX6 boards its working fine and i am able to receive data..

Now how i connect IMX6 board to any of the car's ODB2 port, is there any others connectors are needed or not please explain.

My aim is to connect my IMX6 board to car and get data on CAN bus..

Please explain me..

Thank you.

ラベル(5)
0 件の賞賛
返信
1 返信

1,381件の閲覧回数
art
NXP Employee
NXP Employee

First, you have to connect your i.MX6 board to the CAN bus of the OBD-II connector:

https://en.wikipedia.org/wiki/On-board_diagnostics

Then, you have to study the OBD-II protocol:

https://en.wikipedia.org/wiki/OBD-II_PIDs

And then you have to start entering PIDs from the processor and receiving parameters from the car's ECU and other systems.

You can google much more in the internet on that matter.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信