Combining keypad and touchscreen functions in DirectFB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Combining keypad and touchscreen functions in DirectFB

999 次查看
myke_predko
Senior Contributor III

Hiya,

 

I would like to run an i.MX233 EVK application interfaces to DirectFB using both the LCD touchpanel as well as the eight buttons that are included on the EVK. 

 

I haven't been successful finding example code that brings in the touch panel (DirectFB  was built with the ltib touchscreen option selected) so I decided to go a more basic route and read the touchscreen using the traditional ts functions.  This seems to supersede the (LRADC based) keyboard read,

 

Does anybody have some sample i.MX233 DirectFB code that I could take a look at that accesses the touchpanel so I don't have to include the ts functions and I can run with both the touchscreen and the buttons? 

 

Thanx,

 

myke

标签 (1)
0 项奖励
回复
0 回复数