Hii,
I am working on the Colibri imx6ull 512 mb board, I have configured it as SPI slave configuration and it's working. I need to add DMA to SPI slave so what is the procedure to add DMA in SPI slave mode
Dear Chavira,
I am interested in purchasing an NXP board related to this Colibri imx6ull 512MB IT board, and I would like to inquire about the availability of support and software packages for this particular board.
Could you please guide me on the process for purchasing this board and how I can access the necessary software and support resources from NXP?
Hi @GaganGowda!
We have this board:
The software available for this board is the following:
Best Regards!
Chavira
Dear Chavira,
Thank you for your support. We are planning to purchase the recommended Evaluation kit for the i.MX 6ULL. We intend to work with the Linux operating system on this board, and we would greatly appreciate your assistance in configuring the libraries, toolchain, and other necessary components. Our project involves the continuous acquisition of 24-bit ADC data on the board, operating in SPI master mode. On the other end, we will be using the i.MX 6ULL board to collect data using SPI with DMA in slave mode and send that data to a PC using Ethernet. Please provide any suggestions you may have, and also recommend any NXP System on Module (SoM) based on the NXP i.MX 6ULL ARM Cortex-A7 processor with a CPU clock speed of up to 900MHz.
All the documentation available can be consulted by following the link:
Best Regards!
Chavira
Hello Team,
Is there any update regarding Evaluation kit for the i.MX 6ULL