Codecs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codecs

3,060 Views
GabrielSartori
Contributor II

Hello guys!

 

  My english is not so good but I will try to make myself clear.

  Did anyone try to decode a video using MX28EVK board, gstreamer and freescale codecs?

  I could decode a mpegts streamer using mplayer without hw acceleration but It did not work using gstreamer!

 

  I followed the Linux Multimedia Framwork User Guide!

  My LTIB version is 2.6.35_10.12.01 and the codec package is IMX_MMCODECS_10.12!

 

Thanks in advance!

 

Gabriel Sartori

Labels (1)
0 Kudos
Reply
4 Replies

2,882 Views
tip
Contributor I

Hi Gabriel

I have detected the same problem

Did you find a solution.

NB: libmfwba.so do not exist in my rootfs. - gst-fsl-plugin is selected in ltib.


-peter


Peter nielsen said:



Derek Dai said:

This library belongs to gst-fsl-plugin.

Gabriel de Freitas Sartori said:

I think the problem is that I am missing libmfwba.so!

But I cannot find it anywhere!

 

When I use gstream with options --gst-debug-level=1 I got this message:

 

GST_MFWBUFFER gstmfwbuffer.c:69:open_allocator_dll: Can not open dll, libmfwba.so: cannot open shared object file: No such file or directory.

 

Gabriel Sartori

0 Kudos
Reply

2,882 Views
tip
Contributor I



Derek Dai said:

This library belongs to gst-fsl-plugin.

Gabriel de Freitas Sartori said:

I think the problem is that I am missing libmfwba.so!

But I cannot find it anywhere!

 

When I use gstream with options --gst-debug-level=1 I got this message:

 

GST_MFWBUFFER gstmfwbuffer.c:69:open_allocator_dll: Can not open dll, libmfwba.so: cannot open shared object file: No such file or directory.

 

Gabriel Sartori

0 Kudos
Reply

2,882 Views
DerekDai
Contributor II

This library belongs to gst-fsl-plugin.

Gabriel de Freitas Sartori said:

I think the problem is that I am missing libmfwba.so!

But I cannot find it anywhere!

 

When I use gstream with options --gst-debug-level=1 I got this message:

 

GST_MFWBUFFER gstmfwbuffer.c:69:open_allocator_dll: Can not open dll, libmfwba.so: cannot open shared object file: No such file or directory.

 

Gabriel Sartori

0 Kudos
Reply

2,882 Views
GabrielSartori
Contributor II

I think the problem is that I am missing libmfwba.so!

But I cannot find it anywhere!

 

When I use gstream with options --gst-debug-level=1 I got this message:

 

GST_MFWBUFFER gstmfwbuffer.c:69:open_allocator_dll: Can not open dll, libmfwba.so: cannot open shared object file: No such file or directory.

 

Gabriel Sartori

0 Kudos
Reply