Codec availability on i.MX6ULZ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codec availability on i.MX6ULZ

1,804件の閲覧回数
WPG_Liam
Contributor I

Hi,

This is Liam working for WPG(disty in Korea) as FAE and our customer has several questions about codec. Could you help to get feedback?

Q1) As decoder for playback, all of format below support for?

[Liam] I already reviewd "IMX_LINUX_RELEASE_NOTES" doc but there was no comment about WAV and FLAC codec. 

 - MP3 : 32kHz / 44.1kHz / 48kHz

 - WMA : 32kHz / 44.1kHz / 48kHz

 - WAV : 32kHz / 44.1kHz / 48kHz / 88.2kHz / 96kHz / 176.4kHz / 192kHz

 - FLAC : 32kHz / 44.1kHz / 48kHz / 88.2kHz / 96kHz / 176.4kHz / 192kHz

Q2) As encoder for audio recording, does it support for following formats?

[Liam] There is no comment about audio record in the doc. Does it support?

 - MP3 : 128kbps / 192kbps

Q3-1) As I know, there is no need to aggrement with NXP for using MP3 decoder/encoder. Right?

Q3-2) But I know it requires aggrement with Microsoft for using WMA decoder? Right?

 

Thanks,

Liam

0 件の賞賛
返信
3 返答(返信)

1,785件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

1) Linux 5.15.72 supports WAC and FLAC codecs for more information see the reference manual.

2) Yes, it support mp3 just at 128Kbps

3-1) Correct not agreement.

3-2) Correct!

Regards

0 件の賞賛
返信

1,771件の閲覧回数
WPG_Liam
Contributor I

Hi Bio_TICFSL,

Thanks for your quick feedback.

Customer still wants to know more detail information and document about your feedback.

1) Linux 5.15.72 supports WAC and FLAC codecs for more information see the reference manual.

[Liam] The latest BSP version from NXP is kernel 5.15.71_2.2.0(not 5.15.72), which is released Dec. 2022 and I can't find out audio codec spec. information in the reference manual(v5.15.71). Instead, I can see the audio codec spec. over table 21 of "i.MX Linux Release Note". However, still I am not sure about Q1) since no information in both the release note and reference manual. About your feedabck, let me ask again.

A. How soon the v5.15.72 would be released about?

B. Could you provide the audio codec spec. about your feedback? 

2) Yes, it support mp3 just at 128Kbps

[Liam] Same as above, I can't find out the information about your feedback. 

 

Always thanks,

Liam

0 件の賞賛
返信

1,767件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

There is no more information about codecs, and yes it is the 5.15.71V.

Regards

0 件の賞賛
返信