Codeaurora sources migrated

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codeaurora sources migrated

5,634 Views
BHAVANI_S
Contributor I

Hi All,

It is come to the notice that the sources of imx that were present in the codeaurora site has been closed and the repositories have been moved to the NXP github.

Please let us know the alternative sources for the below mentioned repos in code aurora and the permission required to download them. We are having a high priority release and are blocked because of this.

"https://source.codeaurora.org/external/imx/aosp/"

"https://source.codeaurora.org/external/imx/android-imx" 

"https://source.codeaurora.org/external/imx/" 

Thanks and Regards,

Bhavani S

 

0 Kudos
Reply
4 Replies

5,530 Views
Harvey021
NXP TechSupport
NXP TechSupport

i.mx page at nxp-imx · GitHub and can get updates from release note i.MX Linux Release Notes (nxp.com)

 

Best regards

Harvey

0 Kudos
Reply

3,860 Views
yeswanth
Contributor II

i can't find for the following repositories in github they have similar names, could you mention the exact repositories in github for the following:

name="android-imx"
fetch="https://source.codeaurora.org/external/imx/aosp/"

name="android-imx-orig"
fetch="https://source.codeaurora.org/external/imx/android-imx"

0 Kudos
Reply

5,610 Views
gary_bisson
Senior Contributor III

Hi,

You can find all the Android repositories here:

https://github.com/nxp-imx-android

Regards,

Gary

0 Kudos
Reply

2,802 Views
pholden
Contributor III

I have to build the kirkstone branch of Qoriq Yocto for a client.  I'm getting the following error:

 

eth-config-git-r2 do_fetch: Fetcher failure

 

It's pointing to codeaurora.org.  Where did this package move to?

 

Thanks!

Tags (2)
0 Kudos
Reply