Code Signing Tool hangs when creating encrypted u-boot.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Code Signing Tool hangs when creating encrypted u-boot.

跳至解决方案
1,776 次查看
michalhojsik
Contributor II

Hi.

I am working on encrypted boot on the i.MX6UL using Code Signing Tool (cst) version 2.3 (Code Signing Tool release version BLN_CST_MAIN_02.03.00). 

When I run the code signing tool (version for Linux64) with the following command:

../linux64/cst -o u-boot_csf.bin -c ../crts/SRK2_sha256_2048_65537_v3_usr_crt.pem -i u-boot.csf

using the attached csf source file, the cst tool hangs.

Is there something wrong with the csf file, or it there a bug in the cst?

Regards,

Michal

标记 (1)
0 项奖励
回复
1 解答
1,659 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Michal

please check

https://community.nxp.com/thread/428624 

may be useful to try latest cst 2.3.3 release

https://www.nxp.com/webapp/Download?colCode=IMX_CST_TOOL&appType=license&location=null 

and follow Release_Notes.txt included in package

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,660 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Michal

please check

https://community.nxp.com/thread/428624 

may be useful to try latest cst 2.3.3 release

https://www.nxp.com/webapp/Download?colCode=IMX_CST_TOOL&appType=license&location=null 

and follow Release_Notes.txt included in package

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复