Clarificaton on UART Serial Download Protocol for RT105x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clarificaton on UART Serial Download Protocol for RT105x

2,546 Views
ryanshuttlewort
Contributor IV

Hello I am using MCUXpresso IDE, version v10.1.0 [Build 589] [2017-11-14] with an MIMXRT1050-EVK SDK, version  2.3.0 (2017-11-16).

I am looking for clarification on the UART Serial Download Protocol mentioned in the IMXRT1050RM.pdf document in section 8.9.  The description of the UART protocol details is sparse and then the manual proceeds directly to the description of the USB protocol details in section 8.9.1 with packet descriptions beginning in section 8.9.2 - Serial Download Protocol (SDP).

It is not clear if the UART protocol is identical in command structure to that described in 8.9.2 Serial Download Protocol (SDP).  Adding to this confusion is the mention of the USB HID protocol throughout and possible dependencies on it.

So are the UART and USB protocols identical? 

Do you have any further documentation, example applications, scripts etc. that would assist us in developing our own programming tool?

Are there any limitations we should be aware of when using this approach instead of the MfgTool?

Thanks.

0 Kudos
Reply
1 Reply

1,799 Views
Yuri
NXP Employee
NXP Employee

Hello,

   yes, the UART and USB protocols are identical.

https://community.nxp.com/docs/DOC-1639 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply