Choosing where to run inference from application code - GPU/NPU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Choosing where to run inference from application code - GPU/NPU

ソリューションへジャンプ
1,144件の閲覧回数
StefanoN
Contributor I

Hello.

Normally inference is run on the GPU or NPU based on the USE_GPU_INFERENCE=0/1 env. variable, but I would like to make this choice in code. In the Machine Learning guide it says that that variable is "directly read by the HW acceleration driver".

StefanoN_0-1743595701752.png

Is it feasible to modify the GPU/NPU unified driver to expose this functionality to high abstraction layers? Where can I find it?

If not, What else could I do?

Thanks

 

 

0 件の賞賛
返信
1 解決策
1,095件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @StefanoN!

 

The source code is not public yet, even for us due to the GPU is not an NXP IP, our vendor provides the compiled binary for us.

元の投稿で解決策を見る

4 返答(返信)
1,117件の閲覧回数
StefanoN
Contributor I

I understand. Nonetheless can you help me locate the code for the unified driver?

0 件の賞賛
返信
1,131件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @StefanoN!

Thank you for contacting NXP Support!

 

Unfortunately there is no way to do it different that we mentioned in our MACHINE LEARNING USER GUIDE.

 

Best Regards!

Chavira

0 件の賞賛
返信
1,101件の閲覧回数
StefanoN
Contributor I

My understanding is that the so called NPU/GPU driver is found in the Yocto directory `meta-freescale/recipes-graphics/imx-gpu-viv`, but the SRC_URI is given as `${FSL_MIRROR}/${BPN}-${PV}-${IMX_SRCREV_ABBREV}.bin` which at runtime resolves to `https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-6.4.11.p2.6-aarch64-bc7b6a2.bin`.

Looking in the forum I found this user asking for the source code (https://community.nxp.com/t5/i-MX-Processors/GPU-source-code-with-opencl/m-p/1224323)

It was not public in 2021, is it still not public now?

 

Thanks

0 件の賞賛
返信
1,096件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @StefanoN!

 

The source code is not public yet, even for us due to the GPU is not an NXP IP, our vendor provides the compiled binary for us.