Changing eMMC boot images via Linux on Sabre SDB (II) + MFGTool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Changing eMMC boot images via Linux on Sabre SDB (II) + MFGTool

2,011 Views
controlhorus
Contributor III

Hello

I was trying to flash my custom board eMMC through MFGTool utility. I finally get it working  after many different struggles. One of them was finding the partitioning system from eMMC. This post was at the same time useful and misleading:

Changing eMMC boot images via Linux on Sabre SDB

Several conclusions:

  eMMC has internal registers and can be configured (I did not do it consciously)

  To my kernel, my eMMC is configured to present itself as three differents hard disk devices

     mmcblk0

     mmcblk0boot0

     mmcblk0boot1

  I can write a u-boot-1 in mmcblk0

  I can write another u-boot-2 in mmcblk0boot0

  If mmcblk0boot0 hard disk eMMC drive is not configured as boot partition, imx6 starts from u-boot-1

  If mmcblk0boot0 hard disk eMMC drive is configured as boot partition, imx6 starts from u-boot-2

  The MFGTool-ucl2.xml I have been using is writing the u-boot inside  mmcblk0boot0 and activating this partition as boot partition

  The u-boot.bin and the u-boot.imx are different. The command to write each one of them have different.parameters

Please correct me, if I got something wrong.

Thank you,

Jose

Labels (1)
0 Kudos
Reply
0 Replies