Change resolution at runtime on iMX8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change resolution at runtime on iMX8

4,258 Views
pgentili
Contributor III

Hi everyone,

on our previous system (which was based on imx6dl, yocto krogoth) we were able to support multiple displays for our projects. The displays are connected via LVDS.

Basically we were doing something like this at boot:

  • fbset --timings a b c d e f
  • fbset --geometry a b c d e f
  • /etc/init.d/weston restart

And it worked flawlessy with 3 different displays, with different resolutions.

Now we're trying to implement something similar on imx8mm, yocto sumo. The main difference here is that we are using systemd.

I was expecting to make it work with these steps:

  • fbset --timings a b c d e f
  • fbset --geometry a b c d e f
  • systemctl restart weston

But weston.service is somehow resetting my fbset configuration. This is the message that I get after the service restart:

[ 4724.330511] imx-drm display-subsystem: sn65dsi83_bridge_disable
[ 4724.389148] imx-drm display-subsystem: sn65dsi83_bridge_mode_set: mode: 1280*800@70000
[ 4724.393025] imx-drm display-subsystem: sn65dsi83_bridge_enable
[ 4724.393032] sn65dsi83 3-002c: sn65dsi83_brg_setup
[ 4724.403996] sn65dsi83 3-002c: PIXCLK [ 70000000 ] Hz
[ 4724.404001] sn65dsi83 3-002c: DSI clock [ 420000000 ] Hz
[ 4724.404005] sn65dsi83 3-002c: GeoMetry [ 1280 x 800 ] Hz
[ 4724.408619] sn65dsi83 3-002c: LVDS SINGLE CHANNEL
root@icoremx8mm_alma:~# [ 4725.123157] imx-drm display-subsystem: sn65dsi83_connector_detect
[ 4725.129310] imx-drm display-subsystem: sn65dsi83_connector_get_modes
[ 4725.135728] imx-drm display-subsystem: sn65dsi83_connector_mode_valid: mode: 1280*800@70000 is valid

but the resolution I'm setting with the fbset commands is 1024*798.

I would really not want to write different device trees for each of our diffent product because of maintainability.

Do you have any suggestion to make it work?

Thanks

Paolo Gentili 

0 Kudos
Reply
1 Reply

4,171 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Paolo,

Use the method, please!

-------------------------------------

1.  To change  output mode to your resolution at "/etc/xdg/weston/weston.ini"

      
[output]
name=HDMI-A-1                       
mode=1920x1080@60

 

2. restart weston 

  systemctl restart weston

--------------------------------------

Have a nice day!

B.R,

weidong