Change pins Drive strength runtime

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Change pins Drive strength runtime

1,768件の閲覧回数
nirmalluhana
Contributor IV

Hello,

Release: Yocto-Sumo (4.14.78_1.0.0_GA)

Board: i.MX8MQ based custom board

I want to change pins drive strength runtime without board reboot.

Is it possible to do it? If yes, then what utility or steps I have to follow?

Best regards,

Nirmal

ラベル(1)
タグ(2)
3 返答(返信)

1,686件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nirmal

I am afraid it is not supported in nxp linux bsps, one can try to write to iomux

registers directly from application.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,686件の閲覧回数
nirmalluhana
Contributor IV

Hello Igor,

 

Thanks for your rapid response.

 

Can you please provide more information which application is used for it?

 

Best regards,

Nirmal

0 件の賞賛
返信

1,686件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nirmal

 

there is no special application for it. One can use for example

memtool for adding codes to custom application :

memtool\test - imx-test - i.MX Driver Test Application Software 

 

Best regards
igor

0 件の賞賛
返信