Change pins Drive strength runtime

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change pins Drive strength runtime

1,790 Views
nirmalluhana
Contributor IV

Hello,

Release: Yocto-Sumo (4.14.78_1.0.0_GA)

Board: i.MX8MQ based custom board

I want to change pins drive strength runtime without board reboot.

Is it possible to do it? If yes, then what utility or steps I have to follow?

Best regards,

Nirmal

Labels (1)
Tags (2)
3 Replies

1,708 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nirmal

I am afraid it is not supported in nxp linux bsps, one can try to write to iomux

registers directly from application.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,708 Views
nirmalluhana
Contributor IV

Hello Igor,

 

Thanks for your rapid response.

 

Can you please provide more information which application is used for it?

 

Best regards,

Nirmal

0 Kudos
Reply

1,708 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nirmal

 

there is no special application for it. One can use for example

memtool for adding codes to custom application :

memtool\test - imx-test - i.MX Driver Test Application Software 

 

Best regards
igor

0 Kudos
Reply