Capture 16-bit YUV image data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Capture 16-bit YUV image data

1,397 Views
khang_letruong
Senior Contributor III

Dear Community,

I would like to know if it is possible to use the iMX6Q (or some alternative) for capturing the 16-bit YUV data output from the THC63LVD1024 converter which converts LVDS signal from the Sony FCB-EV9520L camera. 

I saw similar questions but without solutions, however : 

https://community.nxp.com/t5/i-MX-Processors/Could-not-configure-CSI0-bt-1120-on-i-MX6Q/m-p/750813

https://community.nxp.com/t5/i-MX-Processors/imx6q-ipu2-csi-2-16-bit-yuv-video/m-p/898111

 

Thanks in advance and best regards,

Khang

0 Kudos
Reply
8 Replies

1,351 Views
joanxie
NXP TechSupport
NXP TechSupport

pls check your mail

1,314 Views
khang_letruong
Senior Contributor III

Hi @joanxie,

Please check your private message inbox!

Best Regards,

Khang

0 Kudos
Reply

1,288 Views
joanxie
NXP TechSupport
NXP TechSupport

what image do you need for capture? BT1120 interlaced?

0 Kudos
Reply

1,269 Views
khang_letruong
Senior Contributor III

Hi @joanxie,

Attached is the video output of the camera :

FCB-EV9520L.png

 

0 Kudos
Reply

1,267 Views
joanxie
NXP TechSupport
NXP TechSupport

if you connect THC63LVD1024 to imx6q, I need to know what output format you use? is it BT1120?

0 Kudos
Reply

1,245 Views
khang_letruong
Senior Contributor III

Hi @joanxie,

 

According to the attached picture, it is 16-bit YCbCr.

Best Regards,

Khang

0 Kudos
Reply

1,192 Views
joanxie
NXP TechSupport
NXP TechSupport

do you mind sharing more detailed information? the link you attach is about BT1120, if you just use yuv 16bits, imx6q can support it, and how you connect your camera? mipi csi port or parallel port?

0 Kudos
Reply

1,161 Views
khang_letruong
Senior Contributor III

Hi @joanxie,

The camera manufacturer confirmed that its output is compliant with BT709 :

image_2024_01_25T00_25_00_010Z.png

And we plan to connect the camera to the iMX6Q via the THC63LVD1024 to convert LVDS signals to LVCMOS parallel.

Best Regards,
Khang

0 Kudos
Reply