Capacitor for MMPF0100 VINREFDDR pin.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Capacitor for MMPF0100 VINREFDDR pin.

Jump to solution
2,118 Views
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about MMPF0100 connection.

Pelase see Table 4 of MMPF0100 datasheet (Rev.9.0).

It explains about VINREFDDR as following.

=====

VREFDDR regulator input. Bypass with at least 1.0 uF decoupling

capacitor as close to the pin as possible.

=====

However, in MCIMX6DQ-SDP schematics (SPF-27392_C3.pdf), the capacitance for VINREFDDR is less than 1.0 uF since two 0.1 uF capacitors are connected in series.

And 1.0 uF is connected to VREFDDR instead of VINREFDDR.

Which is correct?

Best Regards,

Satoshi Shimoda

Tags (2)
0 Kudos
Reply
1 Solution
2,027 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

necessary capacitance is provided from DDR_1V5 side (connected to

VINREFDDR on SPF-27392 p.19). Also from MMPF0100  p.26 :

Table 20. VREFDDR External Components..

VREFDDR  -- 1.0uF

footnote 30

VINREFDDR to GND, 1.0 uF minimum capacitance is provided by buck regulator output.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,028 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

necessary capacitance is provided from DDR_1V5 side (connected to

VINREFDDR on SPF-27392 p.19). Also from MMPF0100  p.26 :

Table 20. VREFDDR External Components..

VREFDDR  -- 1.0uF

footnote 30

VINREFDDR to GND, 1.0 uF minimum capacitance is provided by buck regulator output.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,027 Views
satoshishimoda
Senior Contributor I

Hi igor,

Thank you for your reply.

OK, I understood the 1.0 uF to VREFDDR is OK.

And according to your reply, I understood the 1.0 uF capacitance written in footnote 30 is provided by C566, C571, C577, and C560 in SPF-27392.

Is this correct?

Best Regards,

Satoshi Shimoda

0 Kudos
Reply
2,027 Views
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes, correct.

Best regards

igor

0 Kudos
Reply