Capacitor for MMPF0100 VINREFDDR pin.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Capacitor for MMPF0100 VINREFDDR pin.

跳至解决方案
2,129 次查看
satoshishimoda
Senior Contributor I

Hi community,

Our partner have a question about MMPF0100 connection.

Pelase see Table 4 of MMPF0100 datasheet (Rev.9.0).

It explains about VINREFDDR as following.

=====

VREFDDR regulator input. Bypass with at least 1.0 uF decoupling

capacitor as close to the pin as possible.

=====

However, in MCIMX6DQ-SDP schematics (SPF-27392_C3.pdf), the capacitance for VINREFDDR is less than 1.0 uF since two 0.1 uF capacitors are connected in series.

And 1.0 uF is connected to VREFDDR instead of VINREFDDR.

Which is correct?

Best Regards,

Satoshi Shimoda

标记 (2)
0 项奖励
回复
1 解答
2,038 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

necessary capacitance is provided from DDR_1V5 side (connected to

VINREFDDR on SPF-27392 p.19). Also from MMPF0100  p.26 :

Table 20. VREFDDR External Components..

VREFDDR  -- 1.0uF

footnote 30

VINREFDDR to GND, 1.0 uF minimum capacitance is provided by buck regulator output.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,039 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

necessary capacitance is provided from DDR_1V5 side (connected to

VINREFDDR on SPF-27392 p.19). Also from MMPF0100  p.26 :

Table 20. VREFDDR External Components..

VREFDDR  -- 1.0uF

footnote 30

VINREFDDR to GND, 1.0 uF minimum capacitance is provided by buck regulator output.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,038 次查看
satoshishimoda
Senior Contributor I

Hi igor,

Thank you for your reply.

OK, I understood the 1.0 uF to VREFDDR is OK.

And according to your reply, I understood the 1.0 uF capacitance written in footnote 30 is provided by C566, C571, C577, and C560 in SPF-27392.

Is this correct?

Best Regards,

Satoshi Shimoda

0 项奖励
回复
2,038 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes, correct.

Best regards

igor

0 项奖励
回复