Cant able to play video via gstreamer using fpsdisplaysink plugin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cant able to play video via gstreamer using fpsdisplaysink plugin

2,128 次查看
manojsampathkum
Contributor II

Hi

I am using the yocto Morty release and 4.9 kernel in that I am trying to play a video using GStreamer along with fpsdisplaysink plugin. But I am unable to play the video . 

 # DEBUG=3 gst-launch-1.0 filesrc location=input.mp4 ! decodebin ! fpsdisplaysink

Setting pipeline to PAUSED ...
display(/dev/fb0) resolution is (1920x1080).
====== OVERLAYSINK:mxc_v4l2_output v4l2_out: Bypass IC.
4.2.1 build on Dec 29 2017 13:15mxc_v4l2_output v4l2_out: Bypass IC.
:48. ======
display(/dev/fb0) resolution is (1920x1080).
display(/dev/fb0) resolution is (1920x1080).
alloc_contig_range: [76000, 763f5) PFNs busy
Pipeline is PREROLLING ...

====== AIUR: 4.2.1 build on Dec 29 2017 13:15:33. ======
Core: MPEG4PARSER_06.09.36 build on Aug 23 2016 05:18:47
file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm11_elinux.so.3.2
------------------------
Track 00 [video_0] Enabled
Duration: 0:00:52.208000000
Language: und
Mime:
video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)1920, height=(int)1080, framerate=(fra
------------------------
------------------------
Track 01 [audio_0] Enabled
Duration: 0:00:51.946000000
Language: und
Mime:
audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)48000, bitrate=(int)0, stream-format=(string)raw, codec_data=(buffer)1190
------------------------

====== BEEP: 4.2.1 build on Dec 29 2017 13:15:37. =alloc_contig_range: [76c00, 770ff) PFNs busy
=====
Core: AAC decoder Wrapperalloc_contig_range: [76c00, 771ff) PFNs busy
build on May 30 2016 12:33:44
alloc_contig_range: [76c00, 772ff) PFNs busy
file: /usr/lib/imx-mm/audio-codealloc_contig_range: [76c00, 773ff) PFNs busy
c/wrap/lib_aacd_wrap_arm12_elinuxalloc_contig_range: [77000, 774ff) PFNs busy
.so.3
CODEC: BLN_MAD-MMCODECS_AACD_ARM_03.09.00_CORTEX-A8 build on Jul 13 2016 18:15:25.
[INFO] bitstreamMode 1, chromaInterleave 0, mapType 0, tiled2alloc_contig_range: [76000, 7637d) PFNs busy
LinearEnable 0
alloc_contig_range: [76000, 7637d) PFNs busy
alloc_contig_range: [76000, 7637d) PFNs busy
alloc_contig_range: [76000, 7637d) PFNs busy
alloc_contig_range: [76000, 7637d) PFNs busy
alloc_contig_range: [76000, 7637d) PFNs busy
alloc_contig_range: [76000, 7637d) PFNs busy
alloc_contig_range: [76000, 7637d) PFNs busy
alloc_contig_range: [76000, 7637d) PFNs busy
alloc_contig_range: [76000, 7637d) PFNs busy
alloc_contig_range: [76000, 7637d) PFNs busy
alloc_contig_range: [76000, 7637d) PFNs busy
alloc_contig_range: [76000, 7637d) PFNs busy
gst-launch-1.0: ../imxvpuapi/imxvpuapi_vpulib.c:2368: imx_vpu_dec_mark_framebuffer_as_displayed: Assertion `framebuffer != NULL' failed.
Aborted.

Is there any patch for this or how to solve this issue.

Hoping for better guidance .

Best regards

Manoj

标签 (4)
标记 (3)
0 项奖励
回复
1 回复

1,659 次查看
joanxie
NXP TechSupport
NXP TechSupport

why need you to use " fpsdisplaysink"? try to use the command "gst-inspect-1.0 | grep fpsdisplaysink", what do you get? what board and bsp version do you use?

0 项奖励
回复