Cannot write SAI register from Linux Kernel Module (IMX6ULZ)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot write SAI register from Linux Kernel Module (IMX6ULZ)

1,443件の閲覧回数
GLavigne
Contributor I

Hello,

We try to write a register (SAI2 Transmit Control Register (I2S2_TCSR)) from a linux kernel module, but for some reason after trying to read the value again, it reads 0. Here is a snippet of the imx6ull.dtsi :

sai2: sai@0202c000 {
                                        compatible = "fsl,imx6ul-sai",
                                                     "fsl,imx6sx-sai";
                                        reg = <0x0202c000 0x4000>;
                                        interrupts = <GIC_SPI 98 IRQ_TYPE_LEVEL_HIGH>;
                                        clocks = <&clks IMX6UL_CLK_SAI2_IPG>,
                                                 <&clks IMX6UL_CLK_DUMMY>,
                                                 <&clks IMX6UL_CLK_SAI2>,
                                                 <&clks 0>, <&clks 0>;
                                        clock-names = "bus", "mclk0", "mclk1", "mclk2", "mclk3";
                                        dma-names = "rx", "tx";
                                        dmas = <&sdma 37 24 0>, <&sdma 38 24 0>;
                                        status = "disabled";
                                };

 And here is the dts we're adding :

&sai2 {
    compatible = "fsl,clock32khz_imx6ulzb2";
    status = "okay";
};


Eventually, here is a part of the module :

#define I2S2_TCSR_ADDR 0x0202C000
#define I2S2_TCSR_VALUE 0xD0000000

#define SAI2_MEM_REGION_SIZE 0x200

static void *pVirtAddr_I2S2_TCSR;

static int clock32khz_probe(struct platform_device *pdev)
{   int value;
        pVirtAddr_I2S2_TCSR=0;

        //SAI2 request mem region
       if(!request_mem_region(I2S2_TCSR_ADDR,SAI2_MEM_REGION_SIZE,"clock32KHz : sai2"))
        {       printk(KERN_ERR "Failed to request mem region I2S2_TCSR_ADDR\n");
                ret=-EBUSY;
                goto ErrSAI2req;
        }

        //I2S2_TCSR
        pVirtAddr_I2S2_TCSR=devm_ioremap_nocache(&pdev->dev,I2S2_TCSR_ADDR,1);
        if(!pVirtAddr_I2S2_TCSR)
        {       printk(KERN_ERR "Failed to remap I/O memory I2S2_TCSR_ADDR\n");
                ret=-ENXIO;
                goto ErrI2S2_TCSR;
        }
        value=*(int *)(pVirtAddr_I2S2_TCSR);
        printk(KERN_INFO "I2S2_TCSR=%X\n",value);
        *(int *)(pVirtAddr_I2S2_TCSR)=I2S2_TCSR_VALUE;

        //TEST
        value=*(int *)(pVirtAddr_I2S2_TCSR);
        printk(KERN_INFO "I2S2_TCSR test1=%X\n",value);
        devm_iounmap(&pdev->dev,pVirtAddr_I2S2_TCSR);
        pVirtAddr_I2S2_TCSR=devm_ioremap_nocache(&pdev->dev,I2S2_TCSR_ADDR,1);
        if(!pVirtAddr_I2S2_TCSR)
        {       printk(KERN_ERR "Failed to remap I/O memory I2S2_TCSR_ADDR\n");
                ret=-ENXIO;
                goto ErrI2S2_TCSR;
        }
        value=*(int *)(pVirtAddr_I2S2_TCSR);
        printk(KERN_INFO "I2S2_TCSR test2=%X\n",value);
        //TEST END

//No error
    return 0;
}
static const struct of_device_id of_clock32khz_match[] = {
        { .compatible = "fsl,clock32khz_imx6ulzb2", },
        {},
};
MODULE_DEVICE_TABLE(of, of_clock32khz_match);

static struct platform_driver clock32khz_device_driver = {
        .probe          = clock32khz_probe,
        .remove         = clock32khz_remove,
        .driver         = {
                .name   = "clock32khz_imx6ulzb2",
                .of_match_table = of_clock32khz_match,
        }
};
module_platform_driver(clock32khz_device_driver);

It seems that everything is working when the module is inserted, but the printk's output is :


I2S2_TCSR test1=D0000000

I2S2_TCSR test2=0

 

Any help would be much appreciated.

Guillaume

0 件の賞賛
返信
1 返信

1,436件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信