Cannot find Qt5Widgets in qt with imx6 solox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot find Qt5Widgets in qt with imx6 solox

1,574件の閲覧回数
gokhansahin
Contributor III

We're working on a project in Qt and using Sabre Solox kit. We're trying to configure the qt settings like this Setting up Qt Creator to build for i.MX6 . However, I didn't compile successfully a project, always get an error like the following image. You can see all setting in qtcreator options. Where do I mistake?

1.JPG2.JPG

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,205件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what bsp version do you use? did you build the qt5 image successfully??

0 件の賞賛
返信

1,205件の閲覧回数
gokhansahin
Contributor III

I'm using L4.1.15_2.0.0-ga and build it successfully with qt image.

0 件の賞賛
返信