Cannot establish serial connection to Sabre AI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cannot establish serial connection to Sabre AI

1,323 次查看
RickJarvis
Contributor I

MCIMX6QAICPU2

I get nothing from UART DEBUG.  On my MacBook when I plug in the DB9 to USB Serial Adapter I see /dev/tty.usbserial.

screen /dev/tty.usbserial 115200

This works when connected to a different device I have.

When powering up or resetting I should see the bootloader logs, yes?

Also, what is the default (boot from SD) setting for S3?

标签 (1)
0 项奖励
回复
2 回复数

1,206 次查看
RickJarvis
Contributor I

I switched to my linux box and dmesg indicates

[485401.375378] usb 3-8: new full-speed USB device number 25 using xhci_hcd
[485401.503840] usb 3-8: New USB device found, idVendor=067b, idProduct=2303
[485401.503844] usb 3-8: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[485401.503846] usb 3-8: Product: USB-Serial Controller D
[485401.503848] usb 3-8: Manufacturer: Prolific Technology Inc.
[485401.504218] pl2303 3-8:1.0: pl2303 converter detected
[485401.504813] usb 3-8: pl2303 converter now attached to ttyUSB0

Still nothing when I use minicom or cutemon. Starting to think I have a bad cable. Will try your "test on PC" suggestion but need to round up the correct DB9 male/female converter..

0 项奖励
回复

1,206 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rick

please check Linux Guide in Linux documentation

https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=13378047864867081... 

and User Guides on

SABRE|Automotive-Infotainment|i.MX6|NXP 

Debug uart communication can be tested on PC with RS232 port.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复