Cannot check DEP/NX flag in imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot check DEP/NX flag in imx6

1,941件の閲覧回数
rockie_love_nxp
Contributor I

Hi all,

I built my image for imx6 board with yocto project that uses meta-freescale bsp.

Currently, we want to check if DEP/NX is enable but cannot find any information from:

dmesg | grep NX

also in cat /proc/cpuinfo, there is no "nx" flag.

processor : 0
BogoMIPS : 10.00
Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd03
CPU revision : 4

processor : 1
BogoMIPS : 10.00
Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd03
CPU revision : 4

processor : 2
BogoMIPS : 10.00
Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd03
CPU revision : 4

processor : 3
BogoMIPS : 10.00
Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd03
CPU revision : 4

I only check the other board S32G with meta-alb but still the same, I cannot check if flag DEP/NX is enable.
Could you please let me know if NXP board support NX bit? Or are there any bugs in BSP?

Thank you

 

0 件の賞賛
返信
3 返答(返信)

1,927件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Neither the S32G and i.MX uses DEP / NX.

DEP is used by default in Ubuntu. This is done via the NX bit if the CPU supports it, or emulated via memory segmentation if the CPU does not support it. For more details, see the non-executable memory feature item.

regards

0 件の賞賛
返信

1,923件の閲覧回数
rockie_love_nxp
Contributor I

Hi Bio_TICFSL,

Thank you for your quick reply. So that means we cannot use DEP feature on i.MX series? Otherwise, should I implement it by myself?
As i read that from armv7, it's already supported XN bit. But I cannot find any method to test if that is used in Linux or not.

0 件の賞賛
返信

1,914件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

in this case you should implement yourself.

Regards

0 件の賞賛
返信