Cannot check DEP/NX flag in imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cannot check DEP/NX flag in imx6

1,942 次查看
rockie_love_nxp
Contributor I

Hi all,

I built my image for imx6 board with yocto project that uses meta-freescale bsp.

Currently, we want to check if DEP/NX is enable but cannot find any information from:

dmesg | grep NX

also in cat /proc/cpuinfo, there is no "nx" flag.

processor : 0
BogoMIPS : 10.00
Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd03
CPU revision : 4

processor : 1
BogoMIPS : 10.00
Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd03
CPU revision : 4

processor : 2
BogoMIPS : 10.00
Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd03
CPU revision : 4

processor : 3
BogoMIPS : 10.00
Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid
CPU implementer : 0x41
CPU architecture: 8
CPU variant : 0x0
CPU part : 0xd03
CPU revision : 4

I only check the other board S32G with meta-alb but still the same, I cannot check if flag DEP/NX is enable.
Could you please let me know if NXP board support NX bit? Or are there any bugs in BSP?

Thank you

 

0 项奖励
回复
3 回复数

1,928 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Neither the S32G and i.MX uses DEP / NX.

DEP is used by default in Ubuntu. This is done via the NX bit if the CPU supports it, or emulated via memory segmentation if the CPU does not support it. For more details, see the non-executable memory feature item.

regards

0 项奖励
回复

1,924 次查看
rockie_love_nxp
Contributor I

Hi Bio_TICFSL,

Thank you for your quick reply. So that means we cannot use DEP feature on i.MX series? Otherwise, should I implement it by myself?
As i read that from armv7, it's already supported XN bit. But I cannot find any method to test if that is used in Linux or not.

0 项奖励
回复

1,915 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

in this case you should implement yourself.

Regards

0 项奖励
回复