Can we send black frames to framebuffer before splash screen appears

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we send black frames to framebuffer before splash screen appears

1,871 Views
praneethreddy46
Fresh Out Contributor

Hi All,

Platform : imx6solo/6Dualite based customized board

kernel: 3.10.17

Can i send black frames to framebuffer before splashscreen(logo) appears ?

If it is possible then how can i pass (black frames) in the driver level ?

Please let me know your views,

Regards,

praneeth L

Labels (2)
0 Kudos
Reply
2 Replies

1,722 Views
Carlos_Musich
NXP Employee
NXP Employee

HI paraneeth,

you may want to customize the splash screen to show a black screen instead the logo. Please take a look to the following thread. How do I customize the splashscreen image in U-boot? 

I hope it helps.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,722 Views
praneethreddy46
Fresh Out Contributor

Hi Musich,

Thanks for your reply.

But  my question is on Linux kernel, there was a flickering just before splash screen(logo) appears, how can i send black frames to frame buffer.

Regards,

praneeth L

0 Kudos
Reply